The bedroom is a personal retreat where individual comfort is of the utmost importance. The Legrand range is specially designed to meet these requirements and offers added safety for the whole family, including the elderly.
The bedroom
Creat a feel - Good atmosphere
Select the desired temperature using a room thermostat, centrally control the light from your bed, use the dimmer to read in the perfect light, and the nightlight function to doze off peacefully. It all makes life so much easier.
Enjoy peace of mind
People who feel safe and secure have a better night’s sleep. Skirting lights with motion detectors or antiglare and downlit pathway lighting will help to prevent any accidents at night. A nightlight can also provide orientation in the dark. A central shutter control for the whole house can help to promote this feeling of security, while a panic scenario switch can also provide reassurance if you hear any suspicious noises.
Connected eco meter
Visibility drives savings: integrated into the distribution board, the connected eco-meter allows to measure consumption of electricity, gas and water and to display it directly on the device, via web pages or through the MyHOME_Screen 10.
Feeling connected is reassuring
Whether they’re set up to respond automatically or at the touch of a button, Legrand assisted living solutions offer a greater sense of independence for the older generation in the event of an emergency.
This feeling of security is heightened by the knowledge that the emergency services will be notified in the event of an incident, for example by a fall detector or by triggering the conspicuous emergency switch.
Universal power supplies
The flush-mounting charger is always available for use, providing freedom from the restrictions of a mobile charger and extending battery life for users on the move.
Céliane intuition
Céliane Intuition - And the light switch off alone.