Skip to main content
Logo print

Immersion Cooling: What is it and key considerations! | Legrand United Kingdom

Immersion Cooling: What is it and key considerations!

Blog 01/10/2025
LegrandData Center White SpaceCooling

What Is Immersion Cooling?

Immersion cooling is a cutting-edge thermal management method where entire servers or IT components are submerged in a thermally conductive, dielectric liquid. This liquid directly absorbs the heat from the hardware, eliminating the need for air cooling, heat sinks, or traditional server fans.

 

There are two primary types of immersion cooling:

  • Single-phase: The liquid stays in liquid form as it absorbs heat, which is then removed via a heat exchanger.
  • Two-phase: The liquid evaporates when it absorbs heat, forming a gas. The gas then condenses back into liquid in a closed loop.

Both methods outperform air and even direct-to-chip cooling in terms of thermal efficiency and rack density potential.

 

Advantages

  • Extreme Density Support: Enables ultra-high-density deployments well beyond what air or even direct-to-chip systems can handle.
  • Superior Thermal Efficiency: Liquid removes heat far more effectively than air. With direct contact cooling, server components remain consistently cool under full load.
  • Silent Operation: Fans are no longer needed in the server, reducing power usage and noise in the data hall.
  • Reduced Mechanical Complexity: Fewer moving parts mean less wear and lower failure rates.
  • Improved Energy Use: Immersion systems often enable Power Usage Effectiveness (PUE) < 1.05, especially in optimized environments.
  • Potential for Heat Reuse: Captured heat can be reused for district heating, industrial processes, or converted into chilled water, aiding sustainability goals.
  • Space Efficiency: Immersion tanks can consolidate massive compute power into a much smaller physical footprint.

 

Considerations and Trade-Offs

Despite its technical appeal, immersion cooling requires a rethinking of how data centers are designed, operated, and serviced:

  • Server Compatibility: Not all IT equipment is immersion-ready. Servers often need to be purpose-built or modified to operate submerged in dielectric fluid.
  • Physical Access and Maintenance: Servicing submerged components can be more complex and time-consuming compared to traditional racks.
  • Operational Culture Shift: Technicians need new workflows, tools, and safety training to handle immersion systems effectively.Fluid Management: Dielectric fluids must be monitored and maintained over time. Disposal and environmental considerations also apply.
  • Limited Industry Standardization: While gaining traction, immersion cooling still lacks some of the maturity and interoperability seen in air or D2C systems.
  • Upfront Investment: Initial CapEx for immersion infrastructure is high, though often offset by long-term energy and space savings.

 

Ideal Use Cases

  • AI & Machine Learning Clusters: Workloads that generate intense, sustained heat benefit from immersion’s consistent cooling performance.
  • HPC Environments: Where performance and density outweigh other concerns, immersion is often the best fit.
  • Edge Computing & Harsh Environments: Immersion systems offer sealed, ruggedized designs ideal for dusty, remote, or temperature-variable locations.
  • New Data Center Designs: Immersion cooling shines in greenfield builds, where infrastructure can be optimized from day one.

 

Conclusion

Immersion cooling represents a transformative leap in data center thermal management though it requires a shift in operations and hardware readiness.