Skip to main content
Logo print

AI and Data Centers: Adapting to High-Density Computing

Blog 06/11/2024
Legrand Data Center Grey Space Racks & Cabinets UPS

The role of UPS solutions for seamless operation is crucial as AI drives higher demands for power, cooling, and storage in modern data centers.

 

AI and Data Centers

With the ongoing surge of digital transformation and the use of generative Artificial Intelligence (AI), we are seeing a massive increase in the adoption of AI applications by businesses to support their growth. According to The World Economic Forum, a third of EU businesses adopted AI in 2023, up 32% from the previous year, with predictions that 75% of businesses will have adopted AI applications by 2030.

The success of these AI applications hinges upon the availability of vast amounts of data, leading to a heightened demand for scalable data center services capable of storing and processing these massive data volumes. As AI applications and workloads escalate power and density requirements, data centers must adapt their design, power infrastructure, and cooling capacities accordingly. A recent report from the International Energy Agency (IEA) predicts that data center energy consumption could double by 2026.

 

Understanding AI and Its Role in Data Center Optimization

Put simply, AI is the technology that enables computers and machines to simulate human intelligence and problem-solving capabilities. In contrast to human capabilities, AI technology excels at identifying patterns, providing insights, and rendering decisions based on vast amounts of data at unparalleled speeds.

Each AI application requires an immense amount of computing power to support its machine learning (ML). The three main applications of ML in data centers are:

  • Optimization of equipment settings: This involves empowering power and cooling systems to dynamically adjust to evolving IT workload demands in near real-time.
  • Predictive analytics: ML facilitates predictive maintenance of data center equipment to mitigate downtime risks and enhance capacity planning accuracy.
  • Anomaly detection: ML aids operations teams in promptly pinpointing the root causes of failures or underperforming equipment, thereby minimizing downtime. Additionally, AI-based enhancements to facility monitoring and physical security systems enable the identification of unauthorized personnel or non-compliant activities.

 

High-Performance Computing (HPC)  

The data needed to support these applications is managed through high-performance computing (HPC) clusters, which consist of multiple servers connected via high-speed networks. This set-up enables parallel processing and faster training times.

  • HPC Design and Power Needs: HPC systems typically fit into standard 19-inch racks, housing servers, networking equipment, and storage arrays. These modular and scalable racks allow easy capacity upgrades. Power density ranges from 20 kW to over 60 kW per rack, requiring robust power, cooling, and backup infrastructure to ensure proper operation.
  • HPC Hardware Components: HPC systems use high-powered processors (CPUs), high-speed memory, and specialized hardware like Graphics Processing Units (GPUs) or Tensor Processing Units (TPUs). These processors perform complex analyses quickly, handling tasks such as scientific simulations, data mining, advanced analytics, and machine learning.

 

HPC Hardware Components

AI’s Impact on Data Storage, Network, and Power Demands

The rise of AI has reshaped various facets of data centers, including data storage, processing, management, and transfer, leading to heightened demands for computing power in both cloud and edge data centers. AI applications need extensive storage for input and output functions, requiring high-speed storage and access for real-time AI workloads.  

Moreover, as AI adoption accelerates, the strain on data center networks becomes more pronounced. AI workloads necessitate high-capacity, error-free networks, putting a strain on data centers' bandwidth and capacity, with large-scale AI applications typically needing about three times more bandwidth than traditional computing networks, especially when components are distributed across multiple servers and storage systems.  

 

AI's Impact on Data Centers

Additionally, the proliferation of AI processors significantly escalates power consumption and density in data centers, presenting unique energy efficiency and sustainability challenges. To address these challenges, data centers are exploring advanced cooling technologies, such as liquid or immersion cooling, to effectively manage increased heat and mitigate the risk of equipment failure.

Maximizing power and cooling capacity and optimizing IT infrastructure for efficiency becomes critical, with a need to integrate flexible and scalable solutions that can adapt to meet these growing requirements.

 

The Crucial Role of UPS in AI-Driven Data Centers

Data center operators are increasingly leveraging AI to enhance operational efficiency, employing AI technologies to monitor hardware, swiftly address equipment issues, optimize energy usage, and regulate temperature and humidity levels. AI is also being used to underpin numerous customer-oriented services, including chatbots, onboarding processes, fraud detection, data visualization, and marketing analytics critical for maintaining customer satisfaction and operational efficiency.

To ensure the continuous operation of these AI-driven services a reliable and constant power supply and robust back-up power protection strategy is essential to prevent disruptions. Emergency power has always been a critical component of data center design, but its importance is magnified in the context of supporting AI applications.

Future AI deployments will demand even more from power infrastructure and data center operators must scale their power strategies to prevent catastrophic data losses and ensure seamless operation. A dependable Uninterruptable Power Supply (UPS) system is not just a precaution; it's a necessity for safeguarding vast volumes of client data and maintaining the integrity of AI-powered services.

Keor FLEX - UPS