What is the highest kW duty achieved by a ColdLogik Rear Door Cooler?
USystems recently launched CL23 HPC Rear Door Cooler is capable of 204kW (14°C / 57°F inlet water).For the medium density requirement, the CL20 is capable of 93kW (14°C / 57°F inlet water). However, using customer specified parameters while on-site, 106kW has been independently tested and verified on the 93kW rated cooler.