How many litres of water does a ColdLogik deployment use?
A ColdLogik RDC design is a closed loop system, so when paired with similar mechanical cooling or other free cooling technologies such as borehole, river, sea water etc is totally sustainable. Which means each deployment only uses water at the initial set-up phase.
The volume of water required at this stage will vary depending on the scale of the intended data centre deployment. The volume capacity of an individual ColdLogik cooler will range between 5.7L (1.5 US Gallons) to 15.4L (4 US gallons) in volume.