Skip to main content
Logo print

How heavy is a ColdLogik Rear Door Cooler?

Depending on the model and dimensions of the Rear Door Cooler, the dry weight will range from between 63.5kg (140lb) to 79.8kg (176lb). Filled weight between 76.2kg (168lb) to 91.2kg (201lb).