Dong Energy's New Build Data Center
Project at a Glance | |
|---|---|
| Location (Date) | Denmark |
| End User | Dong Energy |
| Legrand Solution | USpace ColdLogik compliant 42U cabinets with CL20 C8 Rear Door Heat Exchangers |
| Key Results | Low CAPEX and fast ROI, Low PUE, Low carbon, 340kW cooling capacity, N+1 redundancy |
DONG Energy was established in 2006 by the merger of six Danish energy companies: DONG, Elsam, Energi E2, Nesa, Københavns Energi and Frederiksberg Forsyning. It was created as a vehicle to develop Danish energy activities. The company has expanded significantly through organic growth and acquisitions both in Denmark and across Europe. The merger brought together a wide range of experience, resources, and activities, including oil and natural gas exploration and production, electricity generation at power stations and renewable energy facilities and natural gas and electricity distribution.
Challenge
In 2009 Dong Energy required an energy efficient cutting-edge design for the cooling of their state of the art new build data centre in Denmark.
The site had to retain a small footprint whilst maximising the density and be highly efficient 340kW - for this they requested 15kW - 30kW capacity for each cabinet of the 23 cabinets, including the cooling of 6 IBM SAN cabinets using the same system. The water supply temperature of 15°C was required for the chillers and dry air cooler already chosen for the external space.
The Cooling Solution
How Rear Door Heat Exchangers (RDHx) were Optimized at Dong Energy
USystems installed 17 x USpace ColdLogik compliant 42U cabinets with CL20 C8 rear coolers within the white space of the data centre build. This enabled them the packaging densities required with capacity to increase heat loads in the future within the same footprint. Each rack had the cooling capacity of 7kW to 30kW giving them a total of 340kW.
One of the team’s biggest challenges was to deal with the cooling of the IBM SAN cabinets. The design of these cabinets meant heat would be distributed into the cold aisle - furthermore the enclosure design incorporated an electromagnetic shielding (EMC) which meant that the IBM SAN door had to retain its integrity. To overcome this USystems designed a special rear cooler which incorporated the unique Zero Aisle overhead system which meant the integrity of the IBM SAN door was not compromised.
The external plant comprised of 2 chillers and a dry air cooler which ran at 15°C water temperature were brought together and controlled the entire solution via a small ColdLogik Room Management System (RMS).
As the ColdLogik solution offered a 90% saving on the CRAC based design Dong Energy had previously been quoted for, they have subsequently replaced an existing CRAC based system with ColdLogik CL20’s and are planning further upgrades in the future.
Discover some of our other cases
_____
Data Center Insights: Edition 5
Canada
Latin America (English)
Latin America (Espanol)
USA
China
India
Japan
Republic of Korea
South East Asia (English)
Austria
Belgium
France
Germany
Italy
Netherlands
Spain
Switzerland
Turkey
UK
Africa (english)
Africa (français)
Middle East (english)
Australia
New Zealand