Skip to main content
Logo print

Jaguar Land Rover's Containerised HPC Data Center | Legrand United Kingdom

Case Study

Jaguar Land Rover's Containerised HPC Data Center

 

 

Project at a Glance 

LocationUnited Kingdom
End UserJaguar Land Rover
Legrand SolutionUSpace ColdLogik compliant server cabinets, C12 Rear Door Heat Exchangers
Key ResultsLow CAPEX and fast ROI, Low PUE of 1.2 - 1.26, Low carbon, Major energy savings on CRAC based design, N+1 redundancy

 


Jaguar Land Rover is a company that brings together two much loved, highly prestigious British car brands. After Tata Motors acquired Jaguar and Land Rover from Ford in 2008, it merged the two marques into a single company and its success has flourished, with memorable vehicles and innovative technologies that add to a long-lasting legacy. 

Advanced design, engineering and technology have all played a part in Jaguar Land Rover’s success over the years. The company invests more in research and development than any other manufacturing company in the UK, which has allowed our thousands of world class engineers to develop world-class innovations. It is these breakthroughs that Jaguar Land Rover can rely on to build better-performing vehicles, lower our environmental impact, and inspire customers. ‍

 

 

Challenge

In 2011, Jaguar Landrover required a high density HPC data centre to expand on of their existing data centres in UK, Due to space restrictions this was to be deployed in 3 phases within 40-foot containers. Each container was to house 17 cabinets with a cooling capacity of 10-30kW per cabinet. Therefore, cooling for this project was the priority as there was no false floor, an extremely small footprint, and a serious heat issue with such high densities.

 

The Solution

ColdLogik's Cooling Solutions

How Rear Door Heat Exchangers (RDHx) were Optimized at Jaguar Land Rover


USystems supplied 17 x USpace ColdLogik compliant server cabinets complete with C12 Rear Door Coolers which were deployed within a 40ft container. In total 3 containers (3 phases) each with an identical solution were successfully commissioned for this project enabling the Jaguar Land Rover HPC data centre to be housed in available ‘brown field’ space. The ColdLogik solution offered a major energy saving on a CRAC based design, but also saving the floor footprint and removing the need for a false floor. External plant used was a chiller and dry air cooler which with the ColdLogik Rear Door Coolers enabled a total cooling capacity of 1380kW with a PUE of only 1.2-1.26.


Discover some of our other cases

 

_____

Data Center Insight Ed. 5

Data Center Insights: Edition 5

Data Center Insight Ed. 4

Data Center Insights: Edition 4