Skip to main content
Logo print

Top 10 Reasons to Consider Rear Door Heat Exchangers when Refurbishing Data Centers

Blog 19/05/2026
Legrand USystems Data Center White Space Cooling

AI workloads, rising rack densities, and aging infrastructure are forcing a difficult reality for many operators: your data center wasn’t built for this. 

While headlines focus on hyperscale builds and next-generation campuses, many facilities are still working within existing footprints. In fact, Uptime Institute reports that approximately 50% of data centers are now over a decade old and never designed for today’s thermal loads or dynamic compute demands. 

So how do you modernize without starting from scratch?

 

The Shift Toward Smarter Refurbishment

For many operators, refurbishment, and not rebuild, is the only viable path forward. It’s faster, more sustainable, and far more cost-effective. 

But there’s a catch. 

Traditional cooling methods, such as CRAC and CRAH units, are increasingly struggling to keep up. They rely on predictable airflow and uniform loads, conditions that simply don’t exist in modern, mixed-density environments. 

This is where rear door heat exchangers (RDHx) are gaining serious attention.

 

Cooling at the Source Changes Everything

Instead of conditioning the entire room, RDHx systems remove heat directly at the rack exhaust.

This shift in cooling, bringing it closer to the source, has a ripple effect across the entire facility:

  • More stable and predictable thermal performance

  • Reduced reliance on high airflow and fan speeds

  • Improved efficiency without overcooling

  • Greater flexibility to support higher rack densities 

In short, it’s a smarter way to adapt existing environments to modern workloads.

 

A Practical Path to Higher Density 

One of the biggest challenges in legacy facilities is enabling high-density deployments without major redesign. 

RDHx make this possible by allowing operators to:

  • Introduce high-density racks alongside standard deployments

  • Avoid costly structural changes

  • Scale incrementally, rack by rack 

This is particularly valuable for organizations exploring AI and HPC workloads but not yet ready to adopt full liquid cooling. 

 

Bridging the Gap to Liquid

Cooling Direct liquid cooling is on the horizon, but for many, it’s not yet a practical step.

RDHx offer a low-risk transition point, introducing water-based cooling into the white space in a controlled, manageable way. It’s a stepping stone that builds confidence while preparing infrastructure for what comes next.

 

Why This Matters Now 

Modernization isn’t just about efficiency; it’s about extending the life and value of your existing data center while staying ready for future demands.

Rear door heat exchangers are emerging as a solution that balances:

  • Performance

  • Scalability

  • Risk reduction

  • Cost control 

But that’s only part of the story.

10 key reasons why rear-door heat exchangers are becoming a go-to strategy for data center refurbishment

Discover the Top 10 Reasons to Consider RDHx


We’ve broken down the 10 key reasons why rear-door heat exchangers are becoming a go-to strategy for data center refurbishment, from energy efficiency gains to white space recovery and operational resilience.

Discover More Related Solution Briefs

couv2_ebook_cooling_10_reasons_rdhx_dtc_389x389px.png

Why Rear Door Heat Exchangers Matter in Today’s Liquid Cooling Landscape