The PX4 and PRO4X Rack PDUs - Redefining Hardware Design and Intelligence
Explore how the PX4 and PRO4X Rack PDUs revolutionize data center power management with advanced monitoring, accuracy, and the iX™ Controller platform. Discover the future of rack PDUs today.
Introduction: The Importance of Advanced Power Management
Staying ahead of the curve in today’s fast-paced and highly competitive data center environment requires continuous innovation and improvement. A critical aspect of data center infrastructure is the rack power distribution system, which is crucial to overall performance and uptime. With the all-new PX4 and PRO4X Rack PDUs, businesses can take their power management capabilities to the next level and outperform the competition.
The High Cost of Power Outages
Power is still the main cause of data center outages, leading to significant operational disruption and a heavy financial impact. According to a 2022 global survey, 25% of respondents said their most recent outage incident had cost their organization more than $1 million, both directly and in terms of opportunity and reputation costs. Therefore, data centers require reliable and robust rack power distribution solutions that minimize downtime and prevent power outages.
Advancements in Rack PDU Technology: PX4 and PRO4X
The Raritan PX4 and Server Technology PRO4X Rack PDUs combine advanced hardware and software technology to ensure mission-critical uptime, real-time visibility, and alerts on power performance metrics at the rack or PDU outlet level. These power quality monitoring capabilities are critical to preventing downtime and helping data center professionals to improve efficiency.
Monitoring and Visualization of Power Quality
The PX4 and PRO4X's total harmonic distortion measurement and monitoring features monitor and visualize harmonic events such as voltage dips and swells and crest factor at the rack. In conjunction with waveform capture, organizations can intuitively visualize the power being fed to the PDU or distributed to the PDU's outlets to ensure data center rack power is running efficiently.
Precision Power Usage Monitoring
The PX4 and PRO4X Rack PDUs offer unmatched precision in power usage monitoring, with a ±0.5% metering accuracy that provides extremely accurate and reliable power consumption measurements, critical for data center infrastructure reliability. The PX4 and PRO4X Circuit Breaker Trip Forensics with Waveform Capture feature is another innovative technology that provides intuitive waveform visualizations and data insights to help data center professionals quickly identify which outlet caused a trip, allowing them to proactively take action to prevent future trips, minimizing downtime and avoiding potential losses.
Enhancing Operational Efficiency with iX™ Controller Platform
Another standout feature of the PX4 and PRO4X Rack PDUs is the iX™ Controller platform, which is fully hot-swappable and enables live replacement without disrupting power to connected equipment. This feature reduces downtime risks and minimizes the impact of maintenance activities, allowing businesses to perform necessary maintenance without the risk of costly disruptions.
Conclusion: Optimizing Data Center Operations
The advanced features of the PX4 and PRO4X Rack PDUs provide data center professionals with the ideal solution to optimize their operations. If you want to improve power quality and monitoring in your data center, the PX4 and PRO4X Rack PDUs are the perfect solution.
Learn more about how the PX4 and PRO4X Rack PDUs can help you stay ahead of the competition with the power of forward thinking. For further details on all the capabilities of the new PX4 and PRO4X rack PDUs, explore more.
Explore The Best-In-Class PDUs
Raritan PX4 Rack Power Distribution Unit (PDU)
The PX4 PDU delivers best-in-class intelligence with leading-edge hardware and outlet technology to drive operational excellence.
Server Technology PRO4X Rack Power Distribution Unit (PDU)
The PRO4X PDU offers a revolutionary best-in-class intelligent PDU with leading-edge visibility, reporting, security, and alerting.