Skip to main content
Logo print

NorthC & Legrand: the partnership that makes AI possible | Legrand United Kingdom

NorthC, one of Europe's leading providers of regional data centres, operates Swiss data centres in Münchenstein (Basel), Biel/Bienne (Bern) and Winterthur (Zurich). When a customer requested AI and HPC capacity, this meant NorthC had to quickly upgrade its existing low-density environment at its Münchenstein site near Basel.
By partnering with Legrand, NorthC managed to do so and now offers a scalable, energy-efficient, and reliable high-density infrastructure tailored to the demands of artificial intelligence (AI), big data, and high-performance computing (HPC) workloads. Today, NorthC is an AI enabler that meets every challenge, especially in terms of power supply and cooling. 

Key benefits at a glance!


cust-case_NorthC-Legrand_Icon1_170x90-100

Energy consumption
reduced by up to 80%

image

Improved power usage effectiveness (PUE) for sustainable operations

cust-case_northc-legrand_icon4_170x90-100.jpg

Use of existing infrastructure
 – no costly rebuilds

cust-case_NorthC-Legrand_Icon5_170x90-100

Fast rollout and simple scale-up

cust-case_northc-legrand_project_1440x490.jpg

THE PROJECT

Challenge

Existing NorthC data centers were designed for low-density workloads

New customer requirements: high-density racks (up to 40kW), advanced cooling, compliance with Swiss data laws, and sustainability

Tight timeline: upgrade needed within 6 months

Response

ColdLogik rear door heat exchangers, from Legrand's specialist brand Usystems!

The first intelligent rear door heat exchanger, it now boasts the most energy efficient low to high density rear door cooling solution currently available in the world.

Outcome

Energy consumption reduced by 80% (cooling)

Improved PUE, smaller carbon footprint, and rapid rollout

NorthC now offers AI- and HPC-ready environments, with flexibility for future expansion

Stronger market positioning for both partners as leaders in sustainable, high-performance data center solutions

cust-case_northc-legrand_door-heat_707x710.jpg

THE CUSTOMER'S FEEDBACK


Discover how NorthC transformed its Münchenstein (Basel) site into a high-density, AI- and HPC-ready environment — in just six months.

Watch the full video featuring Wolfgang Voigt, Site Manager at NorthC, and Andreas Bätschmann from Legrand Data Center Solutions Switzerland sharing their insights on the project, the technology behind it, and the strong collaboration that made it a success. 

Adopting the energy-efficient RDHx technology has been a game-changer for us. The fact that it enables high-density computing while reducing energy consumption makes it a compelling choice to meet AI and HPC requirements.

WOLFGANG VOIGT
Münchenstein data center site manager - NorthC

THE SOLUTION

cust-case_northc-legrand_door-heat_707x710.jpg

Rear door heat exchangers


High-tech cooling directly on racks

ColdLogik rear door heat exchangers (RDHx) attach directly to the rear of a server rack. Hot air from the servers flows directly through the exchanger, where it is efficiently cooled by water. Water can absorb over 3,000 times more heat than air. The result? Huge energy savings, improved efficiency, and reliable performance – even under the most demanding AI and HPC workloads.

Using our ColdLogik rear door heat exchangers, we transformed an existing low-density environment into a high-density powerhouse — sustainable, reliable, and ready for AI.

ANDREAS BÄTSCHMANN
Sales Manager for Switzerland - Legrand Data Center Solutions

CONTACT US FOR MORE INFORMATION

Contact us to get more information and to receive a personalized configuration quote! We're committed to providing the best possible service, and we'll work with you to find a solution that meets your needs. 

TRUSTED BY INDUSTRY!

Discover all Legrand Data Center Solutions success stories, providing customers with reliable, efficient and sustainable data center solutions.