Skip to main content
Logo print

Zajil Telecoms's New Build Colocation Data Centre | Legrand United Kingdom

Case Study

Zajil Telecoms's New Build Colocation Data Centre

 

 

Project at a Glance 

LocationKuwait
End UserZajil Telecom
Legrand SolutionUSpace ColdLogik compliant cabinets with ColdLogik CL20 C8 Rear Door Heat Exchangers
Key ResultsLow CAPEX and fast ROI, Low PUE, Low carbon, Modbus monitoring and control application into Zajil’s own Building Management Systems (BMS), Tier 3 (N+1) redundancy

 


Zajil is a leading Information and Communications Technology (ICT) Service Provider in the Middle East & North Africa (MENA) region. Established in the State of Kuwait since 1991, Zajil is Kuwait's first Internet Service Provider and the region's leading MPLS Service Provider. Zajil is a major Data Centre Services player operating multiple data centres in Kuwait, KSA, UAE, Bahrain, Jordan, and UK. Zajil also offers a broad range of Cloud & Managed Services wherein customers rely on Zajil’s expertise to manage their ICT infrastructure. By partnering with global telecom and technology leaders, Zajil provides end-to-end Connectivity, Cloud and Managed Services.

Challenge

In 2013, Zajil International Telecoms were designing their new colocation data centre and required a low energy cooling solution which would be able to expand alongside their growing requirements. They required a phased deployment of cabinets and cooling to keep their capital costs down. The data centre would eventually comprise 80 racks with up to 160kW cooling capacity. With an initial 20 racks and 8 rear ColdLogik Rear Door Coolers with cooling to be added as load increased.

The Cooling Solutions

ColdLogik's Cooling Solutions

How Rear Door Heat Exchangers (RDHx) were Optimized at Zajil


The specification required that the cooling solution would work efficiently on part load. The ColdLogik team designed a modular system which allows for a gradual roll out program. The initial solution required 20 x USpace ColdLogik compliant cabinets with an initial 8 x ColdLogik CL20 C8 Rear Door Coolers. This was supported by three chillers with a water supply temperature of 16°C. This modular approach allows for a growing installation requirement which has been expanded twice within 18 months of the initial installation as their customer base increased. 

Aside from its modularity, the ColdLogik solution was chosen above a cold aisle solution as this was too restrictive in its layout and space utilisation and was not as energy efficient and modular as the customer required. The data centre is currently running at 160kW cooling capacity with an N+1 redundancy rating. A second data centre is planned to utilise the same ColdLogik solutions - Today, Zajil operates two data centres in Kuwait, and one in Saudi Arabia, UAE, Bahrain, and Jordan, as well as a presence in the UK. Its customers are mainly large enterprises and include Kuwait Oil Company and “all major banks in Kuwait”.


Discover some of our other cases

 

_____

Data Center Insight Ed. 5

Data Center Insights: Edition 5

Data Center Insight Ed. 4

Data Center Insights: Edition 4