Skip to main content
Logo print

How does containment support phased expansion?

Containment can be deployed incrementally alongside cabinet installations, meaning the full containment system does not need to be installed at once. 

Phased expansion is most effective when considered during the initial design stage. If future growth is anticipated, the containment layout can be planned with the final configuration in mind, allowing the system to be extended or adapted as the environment evolves without major redesign.