Skip to main content
Logo print

How is fire safety handled in a contained environment?

Fire safety in a contained environment follows the same principles as any other data center design, but the interaction between containment, fire detection, and fire suppression systems must be carefully considered to ensure effective operation within the white space. 

The overall approach depends on how the suppression strategy is implemented. If a dedicated fire suppression system is installed directly within the contained aisle, its operation is generally no different from protection elsewhere in the facility. Where suppression is provided at room level, the containment system must allow the extinguishing agent to reach the aisle. A common solution is the use of drop-away panels or temperature-sensitive components that automatically open at high temperatures, ensuring the suppression system functions as intended.

Compliance and insurance requirements are also important considerations. Components may require recognized certifications, such as FM approval, demonstrating that they have been tested and validated for use in contained environments. These certifications provide assurance to operators, insurers, and designers that fire protection measures will perform reliably.